Solid Edge FrameworkSupport Type Library
UseCustomSheetColor Property
Description
Determines if a custom sheet color is to be used in the window as a backdrop color.
Property type
Read-write property
Syntax
Visual Basic
Public Property UseCustomSheetColor As Boolean
Remarks
If this property is True, the custom color is used. Otherwise, the default Window Background color set in the Control Panel is used. The custom color is define by the CustomSheetColor property.
See Also

BackDrop Object  | BackDrop Members

Send comments on this topic.