Solid Edge FrameworkSupport Type Library
BalloonLeaderTextConnectionPoint Property
Description
Sets and returns the connection point of the leader or breakline to the balloon. Point 0 is at the center, 1 is default left, 2 is default right, 3 and higher are the next points in the clockwise direction from default left.
Property type
Read-write property
Syntax
Visual Basic
Public Property BalloonLeaderTextConnectionPoint As Integer
See Also

Balloon Object  | Balloon Members  | Solid Edge ST5 - What's New

Send comments on this topic.