Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BalloonDirection | Sets and returns the orientation of the referenced Balloon object. |
BalloonDisplayedText | |
BalloonDisplayedTextLower | |
BalloonDisplayedTextPrefix | |
BalloonDisplayedTextSuffix | |
BalloonLeaderTextConnectionPoint | Sets and returns the connection point of the leader or breakline to the balloon. Point 0 is at the center, 1 is default left, 2 is default right, 3 and higher are the next points in the clockwise direction from default left. |
BalloonSides | Sets and returns the number of sides for an N-sided balloon. |
BalloonSize | Sets and returns the size of the referenced Balloon object. |
BalloonText | Sets and returns the text string that is displayed in the referenced Balloon object. |
BalloonTextLower | The lower text that is displayed in the referenced Balloon object. |
BalloonTextPrefix | The prefix text that is displayed in the referenced Balloon object. |
BalloonTextSuffix | The suffix text that is displayed in the referenced Balloon object. |
BalloonType | Sets and returns the shape of the referenced Balloon object. |
BreakLine | Specifies whether or not a breakline is added between the leader line and the referenced dimensioning object. |
BreakLineDirection | Sets and returns the direction (left or right) in which the break line runs along the x axis. |
BreakLineDistance | Sets and returns the length along the x axis that the break line traverses. |
Callout | Specifies whether or not a callout is to be used with the referenced Balloon object. |
CalloutAllAround | Display all around symbol for Callout at the connect point of the leader line and break line. |
CalloutAllOver | Display all over symbol for Callout at the connect point of the leader line and break line. |
CalloutBalloonBreaklineDirection | Sets and returns the breakline direction for callout and balloon. |
CalloutBorder | Callout border displays the border around callout text. Use TRUE to turn ON callout border. |
CalloutBorderHorizontalGap | Callout border horizontal gap. This gap will decide the horizontal spacing between callout border and text on both side and it will override dimension style parameter 'Text clearance gap'. |
CalloutBorderVerticalGap | Callout border vertical gap. This gap will decide the vertical spacing between callout border and text on both side and it will override dimension style parameter 'Vertical box gap'. |
CalloutHorizontalAlignment | Sets and returns the horizontal alignment of callout text. |
CalloutLeaderTextConnectionPoint | Sets and returns the connection point of the leader or breakline to the callout. |
CalloutTextAspectRatio | Callout text aspect ratio. It will be override dimension style parameter for ‘Callout text aspect ratio’. |
CalloutTextWidth | Specifies the width of the callout text. Only used when CalloutWidthFixedAutoAspectRatio or CalloutWidthFixedWrapText is TRUE. |
CalloutTextWidthMode | Gets or sets the text width mode on the callout. CalloutTextWidth should be defined prior to setting to FixedAutoAspectRatio or FixedWrapText. |
DisplayByItemNumber | Specifies whether or not the display of the referenced Balloon object is by item number. |
DisplayItemCount | This read-write Boolean property controls item count display for the referenced Balloon object. |
Document | Returns the document to which the referenced object belongs. |
FSBalloonOverridePrefixText | Gets or sets the overridden prefix text of individual balloon in FS balloon stack. |
FSBalloonOverrideSuffixText | Gets or sets the overridden suffix text of individual balloon in FS balloon stack. |
HidePMI | Show or Hide the referenced PMI Balloon object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Leader | Specifies whether or not the referenced object has a leader line. |
LinkToPartsList | This read-write Boolean property determines whether the referenced Balloon object is linked to a parts list. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
PMIPlane | |
PMITrackDistance | |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
VertexCount | Returns the number of vertices in the referenced object. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |