Solid Edge FrameworkSupport Type Library
DisplayByItemNumber Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Balloon Object
: DisplayByItemNumber Property
Description
Specifies whether or not the display of the referenced Balloon object is by item number.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayByItemNumber As Boolean
Remarks
If set to 1 (True), the display is organized by item number; if 0 (False), it is not.
See Also
Balloon Object
|
Balloon Members
Send comments
on this topic.