Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' getting the CenterLines object on the active sheet
Set objCenterLines = objDoc.ActiveSheet.CenterLines
' drawing a center line on the active sheet
Call objCenterLines.Add(x1:=0.25, y1:=0.15, z1:=0, x2:=0.25, y2:=0.35, z2:=0)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objCenterLines = Nothing
End Sub