| Solid Edge FrameworkSupport Type Library : CenterLines Collection |
Add | Adds an occurrence of the referenced object. |
AddBetweenTwoParallelLines | Creates a CenterLine object between two parallel lines. |
AddByEnd | Creates a CenterLine object from a specified point terminating at a specified object. |
AddByStart | Creates a CenterLine object from a point that starts at a specified object and terminates at a specified coordinate. |
AddByStartEnd | Creates a CenterLine object from a point that starts at a specified ojbect and terminates at another specified object. |
AddCenterArcBy2Arcs | Creates a CenterArc object using two input concentric arcs. |
AddCenterArcBy3Points | Creates a CenterArc object using three input points. |
ClearPlane | Clears any previously set plane object. |
ClearStyle | Clears any previously set style object. |
Item | The items in a collection. |
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |