Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
Dim objCircle1 As SolidEdgeFrameworkSupport.Circle2d
Dim objCircle2 As SolidEdgeFrameworkSupport.Circle2d
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
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' drawing a circle on the active sheet
Set objCircle1 = objDoc.ActiveSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.05)
Set objCircle2 = objDoc.ActiveSheet.Circles2d.AddByCenterRadius(x:=0.5, y:=0.1, Radius:=0.03)
' getting the CenterLines object
Set objCenterLines = objDoc.ActiveSheet.CenterLines
' drawing a center line on the active sheet using the nearest KeyPoints on the Start & End objects
Call objCenterLines.AddByStartEnd(StartObject:=objCircle1, x1:=0.25, y1:=0.5, z1:=0, keyPoint1:=False, _
EndObject:=objCircle2, x2:=0.1, y2:=0.1, z2:=0, Keypoint2:=False)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objCenterLines = Nothing
Set objCircle1 = Nothing
Set objCircle2 = Nothing
End Sub