| Solid Edge FrameworkSupport Type Library > CenterLines Collection : Style Property |
| Visual Basic |
|---|
Public Property Style As DimensionStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines Dim objCLStyle As SolidEdgeFrameworkSupport.DimensionStyle ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If ' getting the CenterLines collection object on the active sheet Set objCenterLines = objDoc.ActiveSheet.CenterLines ' setting the dimension style of the CenterLines collection object to 'ANSI' objCenterLines.Style = objDoc.DimensionStyles(1) ' getting the style object of the CenterLines collection object Set objCLStyle = objCenterLines.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objCenterLines = Nothing Set objCLStyle = Nothing End Sub