Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
    Dim objCenterLine As SolidEdgeFrameworkSupport.CenterLine
    Dim objApplicn As SolidEdgeFrameWork.Application
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' getting the CenterLines object on the active sheet
    Set objCenterLines = objDoc.ActiveSheet.CenterLines
    ' Draw a CenterLine on the active sheet
    Set objCenterLine = objCenterLines.Add(x1:=0.25, y1:=0.15, z1:=0, _
                                           x2:=0.25, y2:=0.35, z2:=0)
    ' Get the Application property
    Set objApplicn = objCenterLine.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterLines = Nothing
    Set objCenterLine = Nothing
    Set objApplicn = Nothing
End Sub
See Also

CenterLine Object  | CenterLine Members

Send comments on this topic.