Solid Edge FrameworkSupport Type Library
CenterLine Object Members
Overview 
Public Methods
Public Method BringForwardChanges the display order of the referenced object by moving it in front of the first object that obscures it.
Public Method BringToFrontChanges the display order of the referenced object by moving it in front of all other overlapping objects.
Public Method ConnectObjectsThis method connects the two specified objects at their respective center lines.
Public Method CopyPlaces a copy of the referenced object on the clipboard.
Public Method CutMoves the referenced object to the system clipboard.
Public Method DeleteDeletes the referenced object.
Public Method GetCenterReturns the object and a point on that object at which the Referenced Arc CenterLine object have center.
Public Method GetCenterPointReturns the point that is the center of the referenced object.
Public Method GetEndReturns the object and a point on that object at which the Referenced CenterLine object terminates.
Public Method GetEndPointReturns the coordinates of the end point of the referenced object.
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetStartReturns the object and a point on that object at which the Referenced CenterLine object starts.
Public Method GetStartPointReturns the coordinates of the start point for the referenced object.
Public Method MoveMoves the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RotateRotates the referenced object about the point specified by the angle in radians.
Public Method ScaleScales the referenced object by a specified factor.
Public Method SelectSelects the referenced object in the active window.
Public Method SendBackwardChanges the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Public Method SendToBackChanges the display order of visible objects by moving the referenced object behind all overlapping objects.
Public Method SetCenterRelocates the center of the referenced Arc CenterLine object.
Public Method SetCenterPointRelocates the center point of the specified object.
Public Method SetEndRelocates the end of the referenced CenterLine object.
Public Method SetEndPointSets the x and y values of the end point for the referenced object.
Public Method SetKeyPointSets the position for a specified key point.
Public Method SetStartRelocates the start of the referenced CenterLine object.
Public Method SetStartPointRelocates the starting point of the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property CenterLineTypeSets and returns the centerline type name for the referenced object.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property IndexReturns the numeric index for the active object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property LayerSets and returns the named layer on which the referenced object resides.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PlaneFor dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object.
Public Property StyleFor collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Public Property TypeSpecifies the type of the object being referenced.
Public Property ZOrderSpecifies the front-to-back order in which an object is displayed relative to other objects.
See Also

CenterLine Object

Send comments on this topic.