Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
    Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objCirc As SolidEdgeFrameworkSupport.Circle2d
    Dim lngZorder1 As Long, lngZorder2 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the CenterMarks collection object on the active sheet
    Set objCenterMarks = objSheet.CenterMarks
    ' Create a CenterMark on the active sheet
    Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
    ' Get the Zorder
    lngZorder1 = objCenterMark.ZOrder
    ' Create a line objcet
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.25, x2:=0.4, y2:=0.25)
    ' Create a circle object
    Set objCirc = objSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
    ' Apply BringForward method to CenterMark object
    Call objCenterMark.BringForward
    ' Get the Zorder
    lngZorder2 = objCenterMark.ZOrder
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterMarks = Nothing
    Set objCenterMark = Nothing
    Set objLine = Nothing
    Set objCirc = Nothing
End Sub