| Solid Edge FrameworkSupport Type Library : CenterMark Object |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
GetArcCenter | This method returns the object that defines the center point of the arc. |
GetArcCenterPoint | Returns the point that is the center of the referenced object. |
GetCenter | For DatumPoints, returns the center point coordinate. For CenterMarks, returns the object and coordinates of the object in which the CenterMark was place. |
GetCenterPoint | Returns the point that is the center of the referenced object. |
GetKeyPoint | Returns information about a specified key point. |
Move | Moves the referenced object. |
PromoteToCurrentVersion | Promotes center mark to the latest version behavior, the same as if placing a new object. |
Range | Returns the high and low range values for the referenced object. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetArcCenter | This method sets the object that defines the center point of the arc. |
SetArcCenterPoint | Relocates the center point of the specified object. |
SetCenter | Specifies a new location for a CenterMark or DatumPoint object. |
SetCenterPoint | Relocates the center point of the specified object. |
SetKeyPoint | Sets the position for a specified key point. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Axis | Sets and returns the object used as the axis for the referenced object. It must be a line. |
ConnectObject | This read-only property returns the object to which the center mark is connected for the referenced CenterMark object. |
Document | Returns the document to which the referenced object belongs. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
TextScale | Sets and returns the text scale of the object. |
TwoPoint | This read-only Boolean property returns True if the referenced CenterMark object is a 2-point centermark. |
Type | Specifies the type of the object being referenced. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |