Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim objCirc As SolidEdgeFrameworkSupport.Circle2d
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
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Create a line objcet
Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
' Create a circle object
Set objCirc = objSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.06)
' Get the CenterMarks collection object on the active sheet
Set objCenterMarks = objSheet.CenterMarks
' Create a CenterMark on the active sheet
Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
' Apply SendBackward method to CenterMark object
Call objCenterMark.SendBackward
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objCenterMarks = Nothing
Set objCenterMark = Nothing
Set objLine = Nothing
Set objCirc = Nothing
End Sub