Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks
Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim objCenter As Object
Dim dblX As Double, dblY As Double, dblZ As Double
Dim bFlag As Boolean
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
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' getting the active sheet
Set objSheet = objDoc.ActiveSheet
' Get the CenterMarks collection object on the active sheet
Set objCenterMarks = objSheet.CenterMarks
' Create a CenterMark on the active sheet
Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0)
' Create a line objcet
Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
' Set the center
Call objCenterMark.SetCenter(CenterObj:=objLine, x:=0.5, y:=0.5, z:=0, Keypoint:=True)
' Get the center
Call objCenterMark.GetCenter(CenterObj:=objCenter, x:=dblX, y:=dblY, z:=dblZ, Keypoint:=bFlag)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objLine = Nothing
Set objCenterMarks = Nothing
Set objCenterMark = Nothing
End Sub