| Solid Edge FrameworkSupport Type Library > CenterMark Object : Style Property | 
| Visual Basic | 
|---|
| Public Property Style As DimStyle | 
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks Dim objCenterMark As SolidEdgeFrameworkSupport.CenterMark Dim objStyle As SolidEdgeFrameworkSupport.DimStyle Dim strVisible As String ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'getting the Active Sheet object Set objSheet = objDoc.ActiveSheet ' Get the CenterMarks collection object on the active sheet Set objCenterMarks = objSheet.CenterMarks ' Create a CenterMark on the active sheet Set objCenterMark = objCenterMarks.Add(x:=0.25, y:=0.25, z:=0) ' Get the object style Set objStyle = objCenterMark.Style ' Get the Linear name property of object strVisible = objStyle.ViewLineType ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objCenterMarks = Nothing Set objCenterMark = Nothing Set objStyle = Nothing End Sub