Solid Edge FrameworkSupport Type Library
ComplexString2d Object Members
Overview 
Public Methods
Public Method AddMemberAdds a two-dimensional geometry object to a ComplexString2d object.
Public Method AddSegmentedStyleDefines a segment on a graphic object and assigns a linear style to that segment.
Public Method BringForwardChanges the display order of the referenced object by moving it in front of the first object that obscures it.
Public Method BringToFrontChanges the display order of the referenced object by moving it in front of all other overlapping objects.
Public Method CopyPlaces a copy of the referenced object on the clipboard.
Public Method CutMoves the referenced object to the system clipboard.
Public Method DeleteDeletes the referenced object.
Public Method DropConverts the referenced object to lower-order elements. For example, converts Rectangle2d objects to four end-point connected, perpendicularly constrained lines.
Public Method DuplicateCopies the referenced object to a specified location, creating a new instance of the object with the same property values as the original.
Public Method GetCentroidReturns the coordinates of the centroid of the referenced object.
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetSegmentedStyleReturns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object.
Public Method MirrorCopies the referenced object about an axis.
Public Method MoveMoves the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RemoveAllSegmentedStylesRemoves all segments defined for the referenced graphic object.
Public Method RemoveMemberRemoves an object previously defined as a member of the referenced ComplexString2d object.
Public Method RemoveSegmentedStyleRemoves the segmented style at the specified index on the graphic.
Public Method RotateRotates the referenced object about the point specified by the angle in radians.
Public Method ScaleScales the referenced object by a specified factor.
Public Method SelectSelects the referenced object in the active window.
Public Method SendBackwardChanges the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Public Method SendToBackChanges the display order of visible objects by moving the referenced object behind all overlapping objects.
Public Method SetKeyPointSets the position for a specified key point.
Public Method SetSegmentedStyleApplies a new linear style to a specified segment on a graphic object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AreaReturns the area of the referenced object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property DrawingObjectsReturns a collection of drawing objects in the referenced group.
Public Property FormReturns the closure state of the referenced object.
Public Property IndexReturns the numeric index for the active object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property LayerSets and returns the named layer on which the referenced object resides.
Public Property LengthSpecifies the length of the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property SegmentedStyleCountReturns the number of segmented styles defined for the referenced graphic object.
Public Property StyleFor collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Public Property TypeSpecifies the type of the object being referenced.
Public Property ZOrderSpecifies the front-to-back order in which an object is displayed relative to other objects.
See Also

ComplexString2d Object

Send comments on this topic.