Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
    Dim objDatumTarget1 As SolidEdgeFrameworkSupport.DatumTarget
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim lngZorderbfr As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Add a Text to the Datum Target
    objDatumTarget.DatumReference = "A"
    'Get the ZOrder before drawing other elements
    lngZorderbfr = objDatumTarget.ZOrder
    'Add a vertex at the end
    Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
    'Draw a Line in the active sheeet
    Set objLine = objSheet.Lines2d.AddBy2Points(X1:=0.2, Y1:=0.4, _
                                                X2:=0.4, Y2:=0.2)
    'Create another Datum target in the active sheet
    Set objDatumTarget1 = objDatumTargets.Add(x1:=0.4, y1:=0.35, z1:=0)
    'Add a Text to the DatumTarget1
    objDatumTarget1.DatumReference = "B"
    'Add a vertex at the end to the DatumTarget1
    Call objDatumTarget1.AddVertex(x:=0.35, y:=0.15, z:=0)
    'Bring forward first Datum Target
    objDatumTarget.BringForward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
    Set objDatumTarget1 = Nothing
    Set objLine = Nothing
End Sub