| Solid Edge FrameworkSupport Type Library : DatumTarget Object |
AddVertex | Creates a vertex at the end of the object. |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
GetAlignmentShape | Returns alignment shape and alignment shape point |
GetDisplayData | |
GetFreeSpacePoint | Returns the coordinates of the terminal connect point for a leader line that belongs to the active dimensioning object. |
GetKeyPoint | Returns information about a specified key point. |
GetTerminator | Returns the object to which the terminal end of a dimensioning or annotation object's leader connects. |
GetVertex | Returns the coordinates of the referenced object based on a specified index. |
GetVertices | Returns an array of vertex coordinates in a dimensioning object. |
InsertVertex | Adds a vertex at a specified index causing indices of following vertices to increment by one. |
Move | Moves the referenced object. |
PromoteToCurrentVersion | Promotes datum target to the latest version behavior, the same as if placing a new object. |
Range | Returns the high and low range values for the referenced object. |
RemoveVertex | Removes a vertex at a specified index, causing indices of following vertices to decrement by one. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetAlignmentShape | Connects annotation to alignment shape at specified point. |
SetFreeSpacePoint | Specifies the coordinates of the terminal connect point for a leader line belonging to the referenced dimensioning object. |
SetKeyPoint | Sets the position for a specified key point. |
SetTerminator | Specifies a new object and/or connect point for the terminal end of an annotatino object's leader. |
SetVertex | Sets the coordinates of an existing vertex of the referenced object. |
SetVertices | Creates vertices in a dimensioning object from an array of x-y coordinates. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BreakLine | Specifies whether or not a breakline is added between the leader line and the referenced dimensioning object. |
BreakLineDirection | Sets and returns the direction (left or right) in which the break line runs along the x axis. |
BreakLineDistance | Sets and returns the length along the x axis that the break line traverses. |
DatumAreaSize | Sets and returns the area of the referenced DatumTarget object. |
DatumAreaSizeDisplay | Specifies whether or not the DatumAreaSize is displayed. |
DatumReference | Sets and returns the datum text for the referenced DatumTarget object. |
DatumTargetType | Sets and returns the datum target type. |
Document | Returns the document to which the referenced object belongs. |
HidePMI | Show or Hide the referenced PMI Datum Target object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Leader | Specifies whether or not the referenced object has a leader line. |
LeaderType | Sets and returns the leader type for the referenced DatumTarget object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PMIPlane | |
PMITrackDistance | |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
VertexCount | Returns the number of vertices in the referenced object. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |