Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
Dim objDatumTarget1 As SolidEdgeFrameworkSupport.DatumTarget
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim lngZorderbfr As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Getting the DatumTargets object
Set objDatumTargets = objSheet.DatumTargets
'Create a Datum target in the active sheet
Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
'Add a Text to the Datum Target
objDatumTarget.DatumReference = "A"
'Get the ZOrder of the DatumTarget befor drawing the other elements
lngZorderbfr = objDatumTarget.ZOrder
'Add a vertex at the end
Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
'Draw a Line in the active sheeet
Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.6, y1:=0.15, _
x2:=0.1, y2:=0.4)
'Create another Datum target in the active sheet
Set objDatumTarget1 = objDatumTargets.Add(x1:=0.25, y1:=0.35, z1:=0)
'Add a Text to the DatumTarget1
objDatumTarget1.DatumReference = "B"
'Add a vertex at the end to the DatumTarget1
Call objDatumTarget1.AddVertex(x:=0.35, y:=0.15, z:=0)
'Bring forward first Datum Target
objDatumTarget.BringToFront
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatumTargets = Nothing
Set objDatumTarget = Nothing
Set objDatumTarget1 = Nothing
Set objLine = Nothing
End Sub