Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
    Dim objAttributeSets As Object
    Dim objAttributeSet As Object
    Dim bAttrPresence As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Set the DatumReference
    objDatumTarget.DatumReference = "A"
    'Add a vertex
    Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
    'Get the AttributeSets of DatumTarget
    Set objAttributeSets = objDatumTarget.AttributeSets
    'Create an AttributeSet
    Set objAttributeSet = objAttributeSets.Add("MyAttrib Set")
    ' Check AttributeSet presence
    bAttrPresence = objDatumTarget.IsAttributeSetPresent("MyAttrib Set")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
    Set objAttributeSets = Nothing
    Set objAttributeSet = Nothing
End Sub