Solid Edge FrameworkSupport Type Library
RemoveVertex Method
Specifies the index, relative to zero of the vertex number in the Linestring. This value must be between one and the number of vertices.
Description
Removes a vertex at a specified index, causing indices of following vertices to decrement by one.
Syntax
Visual Basic
Public Sub RemoveVertex( _
   ByVal Index As Long _
) 
Parameters
Index
Specifies the index, relative to zero of the vertex number in the Linestring. This value must be between one and the number of vertices.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
    Dim lngVertexCount As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Set the DatumReference property
    objDatumTarget.DatumReference = "A"
    'Add a vertex at the end
    Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
    'Add two more vertices
    Call objDatumTarget.AddVertex(x:=0.45, y:=0.2, z:=0)
    Call objDatumTarget.AddVertex(x:=0.4, y:=0.15, z:=0)
    lngVertexCount = objDatumTarget.VertexCount
    'Remove second vertex
    Call objDatumTarget.RemoveVertex(Index:=2)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
End Sub
See Also

DatumTarget Object  | DatumTarget Members

Send comments on this topic.