Solid Edge FrameworkSupport Type Library
SetKeyPoint Method
Specifies the index of the key point/handle.
Specifies the x coordinate of the specified key point.
Specifies the y coordinate of the specified key point.
Specifies the z coordinate of the specified key point.
Description
Sets the position for a specified key point.
Syntax
Visual Basic
Public Sub SetKeyPoint( _
   ByVal Index As Long, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double _
) 
Parameters
Index
Specifies the index of the key point/handle.
x
Specifies the x coordinate of the specified key point.
y
Specifies the y coordinate of the specified key point.
z
Specifies the z coordinate of the specified key point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Set the DatumReference property
    objDatumTarget.DatumReference = "A"
    'Add a vertex at the end
    Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
    'Set the Leader line to true
    objDatumTarget.Leader = True
    'Set the BreakLine to true
    objDatumTarget.BreakLine = True
    'Set the key point
    Call objDatumTarget.SetKeyPoint(Index:=1, x:=0.25, y:=0.3, z:=0)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
End Sub
See Also

DatumTarget Object  | DatumTarget Members

Send comments on this topic.