| Solid Edge FrameworkSupport Type Library > DatumTarget Object : Style Property |
| Visual Basic |
|---|
Public Property Style As DimStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget Dim objStyle As DimStyle ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'getting the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Getting the DatumTargets object Set objDatumTargets = objSheet.DatumTargets 'Create a Datum target in the active sheet Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25) 'Set the DatumReference objDatumTarget.DatumReference = "A" 'Add a vertex Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0) 'Get the style of the datumtarget Set objStyle = objDatumTarget.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objDatumTargets = Nothing Set objDatumTarget = Nothing Set objStyle = Nothing End Sub