Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objDimns As SolidEdgeFrameworkSupport.Dimensions
    Dim objDimAxis As Object
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Line object in the Profile
    Set objL1 = objProfile.Lines2d.AddBy2Points(x1:=0.02, y1:=0.02, x2:=0.034, y2:=0.034)
    Set objDimns = objProfile.Dimensions
    ' Set the Line object as the Axis
    objDimns.Axis = objL1
    'Clear the Axis used for dimensioning
    Call objDimns.ClearAxis
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objL1 = Nothing
    Set objDimns = Nothing
End Sub