AddAngle | Creates a dimension to measure the angle of a line or an arc. |
AddAngleBetween3Objects | Creates an angular dimension between three objects. |
AddAngleBetweenObjects | Creates an angular dimension between two given elements. |
AddAngularCoordinate | Creates a Dimension object for the position of key points or elements from a common origin. |
AddAngularCoordinateOrigin | Creates a Dimension object for the position of key points or elements from a common origin. |
AddChamfer | Creates a dimension to measure the angle and the setback of a chamfer. |
AddCircularDiameter | Creates a dimension to measure the circular diameter of a circle or arc object. |
AddCoordinate | Creates a Dimension object for the angular position of key points from a common origin. |
AddCoordinateEx | Creates a Dimension object for the angular position of key points from a common origin. |
AddCoordinateOrigin | Creates a Dimension object for the angular position of key points from a common origin. |
AddCoordinateOriginEx | Creates a Dimension object for the angular position of key points from a common origin. |
AddDimension | Creates a dimension. For creating PMI dimensions a plane must be set (XY plane is the default). The type of the dimension, the number of parents, and the collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of dimensions. |
AddDistanceBetweenObjects | Creates a dimension to measure distance between two specified objects. |
AddDistanceBetweenObjectsEX | This method creates a dimension to measure distance between two specified objects with tangency options. |
AddDistanceIntersectionToIntersection | Adds a dimension to measure distance between two specified intersections. |
AddDistanceIntersectionToObject | Adds a dimension from an intersection to a key point on an object. |
AddDistanceObjectToIntersection | Adds a dimension from a key point on an object to an intersection. |
AddLength | Creates a dimension to measure the length of a line or an arc. |
AddRadialDiameter | Creates a dimension to measure the radial diameter of a Circle2d or Arc2d object. |
AddRadius | Creates a dimension to measure the radius of a Circle2d or an Arc2d object. |
AddSymmetricalDiameter | Adds a symmetrical diameter dimension to measure distance between two objects. |
ClearAxis | Clears any previously set axis. |
ClearPlane | Clears any previously set plane object. |
ClearStyle | Clears any previously set style object. |
Item | The items in a collection. |