Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objDimns As SolidEdgeFrameworkSupport.Dimensions
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objD1 As SolidEdgeFrameworkSupport.Dimension
    Dim lngCnt As Long
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Line object in the Profile
    Set objL1 = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    ' Create a Dimensions Collection object
    Set objDimns = objProfile.Dimensions
    ' Add a Dimension object to the Collection
    Set objD1 = objDimns.AddLength(Object:=objL1)
    ' Get the Count Property
    lngCnt = objDimns.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objDimns = Nothing
    Set objD1 = Nothing
    Set objL1 = Nothing
End Sub