Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objline As SolidEdgeFrameworkSupport.Line2d
    Dim objDimension As SolidEdgeFrameworkSupport.Dimension
    Dim bAngleComp As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a Line object
    Set objline = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.3, _
                                                x2:=0.3, y2:=0.1)
    'create dimension for the arc2d object
    Set objDimension = objSheet.Dimensions.AddAngle(Object:=objline)
    'check/read whether the angle is clockwise
    bAngleComp = objDimension.AngleCompliment
    'set property anglecompliment
    objDimension.AngleCompliment = True
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objline = Nothing
    Set objDimension = Nothing
End Sub