Solid Edge FrameworkSupport Type Library
KeyPointCount Property
Description
Returns the number of keypoints/handles that are supported by the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property KeyPointCount As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objline As SolidEdgeFrameworkSupport.Line2d
    Dim objdims As SolidEdgeFrameworkSupport.Dimensions
    Dim objDimension As SolidEdgeFrameworkSupport.Dimension
    Dim LngKeyPointCount As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create an line2d
    Set objline = objSheet.Lines2d.AddBy2Points(0.1, 0.1, 0.3, 0.1)
    'create Dimension collection
    Set objdims = objSheet.Dimensions
    'create an coordinate dimension origin
    Set objDimension = objdims.AddCoordinateOrigin(Object:=objline, _
                                                   x:=0.1, y:=0.1, z:=0, KeyPoint:=True)
    'get keypointcount for dimension
    LngKeyPointCount = objDimension.KeyPointCount
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objdims = Nothing
    Set objDimension = Nothing
    Set objline = Nothing
End Sub
See Also

Dimension Object  | Dimension Members

Send comments on this topic.