Solid Edge FrameworkSupport Type Library
SecondaryUpperTolerance Property
Description
Sets and returns the text for the secondary upper tolerance value.
Property type
Read-write property
Syntax
Visual Basic
Public Property SecondaryUpperTolerance As String
Remarks
The SecondaryToleranceEquivalent property of the DimStyle object should be set to False before you set SecondaryUpperTolerance. Otherwise, nothing will happen.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objline As SolidEdgeFrameworkSupport.Line2d
    Dim objDim As SolidEdgeFrameworkSupport.Dimension
    Dim ObjDimStyle As SolidEdgeFrameworkSupport.DimStyle
    Dim strSecUppTol As String
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a line
    Set objline = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.3, y2:=0.3)
    'create a dimension object
    Set objDim = objSheet.Dimensions.AddLength(Object:=objline)
    'get dim style of the dimension
    Set ObjDimStyle = objDim.Style
    'set DualDisplay property of dimstyle to true
    ObjDimStyle.DualDisplay = True
    'set the dimension display type to tolerance
    objDim.DisplayType = igDimDisplayTypeTolerance
    'Set the Primary Upper and Lower Tolerances. If the Primary tolerances are not set
    'secondary tolerances are not displayed.
    objDim.PrimaryUpperTolerance = "0.01"
    objDim.PrimaryLowerTolerance = "0.01"
    'get SecondaryUpperTolerance
    strSecUppTol = objDim.SecondaryUpperTolerance
    'set SecondaryUpperTolerance
    objDim.SecondaryUpperTolerance = "0.04"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objline = Nothing
    Set objDim = Nothing
    Set ObjDimStyle = Nothing
End Sub
See Also

Dimension Object  | Dimension Members

Send comments on this topic.