Solid Edge FrameworkSupport Type Library
SetJogPoint1Distance Method
Specifies the JogPoint1 distance along the dimension line.
Description
Sets the JogPoint1 distance for the jogged line in a Dimension.
Syntax
Visual Basic
Public Sub SetJogPoint1Distance( _
   ByVal Value As Double _
) 
Parameters
Value
Specifies the JogPoint1 distance along the dimension line.
Remarks
This method is applicable only for dimensions with jogged capability (for example, all radius, diameter, and coordinate dimensions).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArc As SolidEdgeFrameworkSupport.Arc2d
    Dim objDimension As SolidEdgeFrameworkSupport.Dimension
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create an arc2d
    Set objArc = objSheet.Arcs2d.AddByCenterStartEnd(xCenter:=0.2, _
                                                     yCenter:=0.2, xStart:=0.1, yStart:=0.1, xEnd:=0.3, yEnd:=0.3)
    'create a dimension
    Set objDimension = objSheet.Dimensions.AddRadius(Object:=objArc)
    'set the jogged property
    objDimension.Jogged = True
    'SetJogPoint1Distance
    Call objDimension.SetJogPoint1Distance(Value:=0.5)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDimension = Nothing
    Set objArc = Nothing
End Sub
See Also

Dimension Object  | Dimension Members

Send comments on this topic.