AttributeSets | Returns the AttributeSets collection object for the referenced object. |
CaptionAnnotation | Sets and returns the caption string to be used by the specified view annotation type. |
CaptionPrimary | Sets and returns the primary caption source string to be used by the specified view type. |
CaptionSecondary | Sets and returns the secondary caption source string to be used by the specified view type. |
CodeASSuffix | Sets and returns the Suffix (%AS) source string for the specified view type. This is intended for use in a form like VA-VA and may include other formatting options, e.g. “()”. |
CodeLNAnnotationSheetNumber | Sets and returns the Annotation Sheet Number (%LN) source string. This is intended for use with %{Annotation Sheet Number|DV} property text and may include other formatting options, e.g. “()”. |
CodeVNViewSheetNumber | Sets and returns the View Sheet Number (%VN) source string. This is intended for use with %{View Sheet Number|DV} property text and may include other formatting options. |
CodeVRViewRotationAngle | Sets and returns the View Rotation Angle (%VR) source string. This is intended for use with %{View Angle|DV} property text and may include other formatting options. |
CodeVSViewScale | Sets and returns the View Scale (%VS) source string. This is intended for use with %{Primary Scale|DV} and/or %{Secondary Scale|DV} property text and may include other formatting options. |
CPLCaptionLocation | Sets and returns the caption location of the cutting plane line display. |
CuttingPlaneLineArrowOffset | Sets and returns offset distance (0.0 - 1.0) for the arrow terminator. |
CuttingPlaneLineDisplay | Sets and returns the direction of the terminator. |
CuttingPlaneLineDisplayStyle | Sets and returns the display style for the cutting plane. |
Description | Returns a user-specified description of the referenced object. |
DimensionStyle | Sets and returns the dimension style referenced by the drawing view style for settings not defined within the drawing view style itself. Used by property text in captions. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Sets and returns the name of the parent style. |
PrimaryCaptionColor | Sets and returns the color in which PrimaryCaption is displayed. |
PrimaryCaptionFont | Sets and returns the name of the PrimaryCaption’s font. |
PrimaryCaptionFontStyle | Sets and returns the style of the font for the PrimaryCaption. |
PrimaryCaptionTextAlignment | Sets and returns text alignment used for the PrimaryCaption. |
PrimaryCaptionTextAutoFillBackground | Sets and returns whether background color is used for the PrimaryCaption. |
PrimaryCaptionTextSize | Sets and returns the text size for the PrimaryCaption. |
SecondaryCaptionColor | Sets and returns the color in which SecondaryCaption is displayed. |
SecondaryCaptionFont | Sets and returns the name of the SecondaryCaption’s font. |
SecondaryCaptionFontStyle | Sets and returns the style of the font for the SecondaryCaption. |
SecondaryCaptionTextAlignment | Sets and returns text alignment used for the SecondaryCaption. |
SecondaryCaptionTextAutoFillBackground | Sets and returns whether background color is used for the SecondaryCaption. |
SecondaryCaptionTextSize | Sets and returns the text size for the SecondaryCaption. |
ShowAnnotationCaption | Sets and returns whether the caption string is shown for the specified view annotation type. |
ShowCodeASSuffix | Sets and returns the display directive for the Suffix (%AS) source string for the specified view type. |
ShowCodeLNAnnotationSheetNumber | Sets and returns the display directive for the AnnotationSheetNumber (%LN) source string. |
ShowCodeVNViewSheetNumber | Sets and returns the display directive for the ViewSheetNumber source string. |
ShowCodeVRViewRotationAngle | Sets and returns the display directive for the View Rotation Angle source string. |
ShowCodeVSViewScale | Sets and returns the display directive for the View Scale source string. |
ShowPrimaryCaption | Sets and returns whether the primary caption is shown for the specified view type. |
ShowPrimarySecondayCaptionSeparator | Sets and returns the display status of the separator line between the primary and secondary captions. |
ShowSecondaryCaption | Sets and returns whether the secondary caption is shown for the specified view type. |
TerminatorDisplay | Sets and returns the terminator display. |
TerminatorSize | Sets and returns the size of the terminator for the referenced DrawingViewStyle object. |
TerminatorType | Sets and returns the type of terminator for both origin and measure. |
ThickLineLengthRatio | Sets and returns multiplication factor for the line length. Ex. line length = ThickLineLengthRatio x font size. |
ThinTerminatorLines | Sets and returns the thin/thick direction lines of cutting plane line or view plane lines. |
ViewAnnotationLineType | Sets and returns the name of the line type of the viewing and cutting plane lines. |
ViewAnnotationLineWidth | Sets and returns the line width of the viewing and cutting plane lines. |
ViewBorderLineType | Sets and returns the name of the line type of the drawing view border. |
ViewBorderLineWidth | Sets and returns the line width of the drawing view border. |
ViewCaptionLocation | Sets and returns the caption location of the drawing view. |
ViewPlaneLineDisplay | Sets and returns the number of terminator lines displayed for view plane. |
ViewSheetNumberLocation | Sets and returns the Sheet Number Location of the view plane. |
VPLCaptionAtEnd | Sets and returns the caption location of the view plane. |