AddAutoConstraints | |
AddChamfer | Creates a chamfer relationship between a Line2d object and the two objects it intersects. |
AddColinear | Adds a colinear relationship to a Relations2d collection. |
AddConcentric | Adds a concentric relationship to a Relations2d collection. |
AddEqual | Adds an equal relationship to a Relations2d collection. |
AddEqualDirection | This method adds a relationship to the referenced Relations2d collection in which the two specified objects have equal direction at the specified keypoints. |
AddEqualDirectionEqualCurvature | This method adds a relationship to the referenced Relations2d collection in which the two specified objects have equal direction and equal curvature at the specified keypoints. |
AddFillet | Creates a fillet relationship between an Arc2d object and the two objects it intersects. |
AddFix | Adds a fix relationship to a Relations2d collection. |
AddHorizontal | Adds a horizontal relationship to a Relations2d collection. |
AddHorizontalAlign | Adds a horizontal alignment relationship to a Relations2d collection. |
AddIntersection | Adds an intersection relationship to a Relations2d collection. |
AddKeypoint | Adds a key point relationship to a Relations2d collection. |
AddKeypointFix | Adds a Fix relationship (called a Lock relationship in the Solid Edge user interface) to a keypoint of an object. A Fix relationship eliminates two degrees of freedom when placed on a keypoint of a geometric element. |
AddLink | Adds a link relationship to a Relations2d collection. |
AddParallel | Adds a parallel relationship to a Relations2d collection. |
AddPerpendicular | Adds a perpendicular relationship to a Relations2d collection. |
AddPointOn | Adds a point-on relationship to a Relations2d collection. |
AddPointOnCompoundCurve | This method adds a point-on relationship to the referenced Relations2d collection. The method creates a point-on relationship between the key point index of the specified object to a point on the specified compound curve. |
AddSet | Adds a set relationship to a Relations2d collection. |
AddSymmetric | Adds a symmetric relationship to a Relations2d collection. |
AddTangent | Adds a tangent relationship to a Relations2d collection. |
AddTangentBetweenCompoundCurves | This method adds a tangent relationship to the referenced Relations2d collection. The method creates a tangent relationship between two specified compound curves. Each set of curves must be endpoint-connected through keypoint constraints. |
AddTangentEqualCurvature | This method adds a relationship to the referenced Relations2d collection in which the two specified objects are tangent and have equal curvature at the specified keypoints. |
AddVertical | Adds a vertical relationship to a Relations2d collection. |
AddVerticalAlign | Adds a vertical alignment relationship to a Relations2d collection. |
Item | The items in a collection. |