Holds properties to be used to determine the behavior of a SmartFrame2d object.
Object Model
Remarks
Many of the properties are used only by commands that create and manipulate a Smart Frame. These commands are not used by the SmartFrame2d object internally. The BehaviorDefaults property returns an object that contains a list of properties that are not reapplied to the SmartFrame2d after seeding it the first time. (That is, if these properties change, objects that used the properties are not changed.)