Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BehaviorDefaults | Returns the SmartFrame2dDefaults object for the referenced SmartFrame2d object. |
BorderColor | Sets and returns the color of the border when the BorderVisible property is True. |
BorderDashTypeName | Sets and returns the line style to use for the border of the referenced frame object. |
BorderPrinted | Specifies whether or not the border of the referenced frame object is to be printed when the container is printed. |
BorderVisible | Specifies whether or not the border of the referenced frame object is visible. |
BorderWidth | Sets and returns the width of the line used to draw the border of the referenced frame object. |
ContentsVisible | Specifies whether or not the contents of the referenced SmartFrame object are to be displayed. |
CropBottom | Sets and returns the distance from the origin of the referenced object to the bottom of the frame or view. |
CropLeft | Sets and returns the distance from the origin of the referenced object to the left side of the frame or view. |
CropRight | Sets and returns the distance from the origin of the referenced object to the right side of the frame or view. |
CropTop | Sets and returns the distance from the origin of the referenced object to the top of the frame or view. |
FrameDefaults | Returns a Frame object that contains the default visual properties of the Frame's border and background. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsLinkPublic | Specifies whether or not the file associated with the referenced SmartFrame object is public. |
LocateChildren | Specifies whether or not the associated SmartFrame can be located by a spot anywhere within the range of the SmartFrame. |
Margin | Sets and returns the minimum distance from the extents of the OLE object to the extents of the frame boundary. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Placement | Sets and returns the preferred method of placement for the referenced SmartFrame2d object. |
Printed | Specifies whether or not the OLE object (and its frame) is printed when the container is printed. |
ProtectFromSelection | Specifies whether or not the referenced object can be selected by a mouse click. |
Rotation | For OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines. |
ScaleFactor | Sets and returns the scale factor between an object and its source document. |
ShapeOption | Sets and returns the shape for the border of the referenced object. |
SizeMode | Sets and returns the mode that defines what the frame should do when the OLE object's extents change. |
Type | Specifies the type of the object being referenced. |
UpdateOption | Sets and returns the update status of an OLE object when the source is modified. |