Solid Edge FrameworkSupport Type Library
AutomaticLinkUpdate Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2d Object
: AutomaticLinkUpdate Property
Description
Determines the behavior of the OLE object if it is linked in the frame.
Property type
Read-write property
Syntax
Visual Basic
Public Property AutomaticLinkUpdate As Boolean
See Also
SmartFrame2d Object
|
SmartFrame2d Members
Send comments
on this topic.