Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
AutomaticLinkUpdate | Determines the behavior of the OLE object if it is linked in the frame. |
BorderColor | Sets and returns the color of the border when the BorderVisible property is True. |
BorderDashTypeName | Sets and returns the line style to use for the border of the referenced frame object. |
BorderPrinted | Specifies whether or not the border of the referenced frame object is to be printed when the container is printed. |
BorderVisible | Specifies whether or not the border of the referenced frame object is visible. |
BorderWidth | Sets and returns the width of the line used to draw the border of the referenced frame object. |
ContentsVisible | Specifies whether or not the contents of the referenced SmartFrame object are to be displayed. |
CropBottom | Sets and returns the distance from the origin of the referenced object to the bottom of the frame or view. |
CropLeft | Sets and returns the distance from the origin of the referenced object to the left side of the frame or view. |
CropRight | Sets and returns the distance from the origin of the referenced object to the right side of the frame or view. |
CropTop | Sets and returns the distance from the origin of the referenced object to the top of the frame or view. |
Description | Returns a user-specified description of the referenced object. |
DisplayType | Sets and returns the display type for the referenced object. |
Document | Returns the document to which the referenced object belongs. |
Frame | Returns the Frame object for the referenced SmartFrame2d object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsLink | Specifies whether or not the file associated with the referenced SmartFrame2d object was inserted as an OLE link. |
IsLinkPublic | Specifies whether or not the file associated with the referenced SmartFrame object is public. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Margin | Sets and returns the minimum distance from the extents of the OLE object to the extents of the frame boundary. |
Name | Returns the name of the referenced object. |
Object | Returns the dispatch interface associated with the site. |
ObjectType | Returns the type of the object contained in the referenced SmartFrame2d object. |
ObjectVerbsCount | Returns the number of verbs supported by the referenced object. |
Parent | Returns the parent object for the referenced object. |
ProtectFromSelection | Specifies whether or not the referenced object can be selected by a mouse click. |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
ScaleFactor | Sets and returns the scale factor between an object and its source document. |
ShapeOption | Sets and returns the shape for the border of the referenced object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Type | Specifies the type of the object being referenced. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |