Solid Edge FrameworkSupport Type Library
Margin Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2d Object
: Margin Property
Description
Sets and returns the minimum distance from the extents of the OLE object to the extents of the frame boundary.
Property type
Read-write property
Syntax
Visual Basic
Public Property Margin As Double
Remarks
The distance is specified in container units.
See Also
SmartFrame2d Object
|
SmartFrame2d Members
Send comments
on this topic.