Solid Edge FrameworkSupport Type Library
HorizontalAlignment Property
Description
Sets and returns the horizontal alignment of the text within a paragraph.
Property type
Read-write property
Syntax
Visual Basic
Public Property HorizontalAlignment As TextHorizontalAlignmentConstants
Remarks
The horizontal alignment can be left-aligned, right-aligned or center aligned. Valid values are members of the TextHorizontalAlignmentConstants constant set. The TextEdit object always has an insert index or an active selection set. Setting any property on the TextEdit object applies to the current selection set, if one is present, or to the text at the current insert index.
See Also

TextEdit Object  | TextEdit Members

Send comments on this topic.