|  AfterSpacing | Sets and returns the amount of space below the first line of the paragraph for the referenced text object. | 
|  AspectRatio | Sets and returns the character width-to-charager height ratio. | 
|  BeforeSpacing | Sets and returns the amount of space above the first line of the paragraph for the referenced text object. | 
|  Bold | Specifies whether or not the associated text is bold. | 
|  Bullet | Specifies whether or not paragraph bulleting is turned on. | 
|  Characters | Sets and returns character data for the referenced TextEdit object. | 
|  CharacterSpacing | Sets and returns the spacing between characters for the associated text. | 
|  Color | Sets or returns the color of the referenced text. | 
|  FirstLineIndent | Sets and returns the distance from the margin to the start of the line. | 
|  Font | Sets and returns the name of the font. | 
|  HorizontalAlignment | Sets and returns the horizontal alignment of the text within a paragraph. | 
|  InsertIndex | Sets and returns the index at which the next character will be inserted for the referenced TextEdit object. | 
|  IsEmpty | Specifies whether or not the referenced object is empty. | 
|  Italic | Specifies whether or not the associated text is italic. | 
|  Language | Sets and returns the language in which the text is written. | 
|  LeftIndent | Sets and returns the distance from the left margin to the end of the line. | 
|  LineSpacing | Sets and returns the amount of space between two lines in a paragraph for the referenced object. | 
|  LineSpacingType | Sets and returns the Line Spacing type for the referenced TextBox object. | 
|  Name | Returns the name of the referenced object. | 
|  Number | Specifies whether or not paragraph numbering is turned on. | 
|  NumberingStartValue | Sets the start value for the referenced numbered list | 
|  RightIndent | Sets and returns the distance from the right margin to the end of the line. | 
|  SpecialIndentType | Sets and returns the Special Indent type None, First line, or Hanging | 
|  SubScript | Specifies whether or not the associated text is subscripted. | 
|  SuperScript | Specifies whether or not the associated text is superscripted. | 
|  TextScale | Sets and returns the text scale of the object. | 
|  TextSize | Sets and returns the size of the text for the referenced object. | 
|  UnderLine | Specifies whether or not the associated text is underlined. | 
|  VerticalPosition | Sets and returns the vertical position of superscript and subscript text. |