Sets and returns the distance from the left margin to the end of the line.
Property type
Read-write property
Syntax
Visual Basic
Public Property LeftIndent As Double
Remarks
The TextEdit object always has an insert index or an active selection. Setting any property on the TextEdit object applies to the current selection, if one is present, or to the text at the current insert index.