|  ActiveDocument | Returns the currently active document. | 
|  ActiveDocumentType | Returns the type of the currently active document. | 
|  ActiveEnvironment | Returns the environment that belongs to the current active window of the document. | 
|  ActiveObject | Returns an Object from the active document. The type of object returned is specified by Type. | 
|  ActivePrinter | Returns the name of the active printer. | 
|  ActiveSelectSet | Returns the SelectSet object for the currently active window. | 
|  ActiveStatusBarPart | Sets and returns the current active status bar part. | 
|  ActiveWindow | Returns the active Window object. | 
|  AddIns | Returns the AddIns object for the referenced Application object. | 
|  Application | Returns the active application object. | 
|  ApplicationEvents | Returns the ApplicationEvents object for the referenced Application object. | 
|  ApplicationV8AfterDocumentOpenEvent | Returns the ApplicationV8DocumentOpenEvent object for the referenced Application object. | 
|  ApplicationWindowEvents | Returns the ApplicationWindowEvents object for the referenced Application object. | 
|  ApprenticeMode |  | 
|  Caption | Sets and returns the caption of the referenced object. | 
|  Customization | An object that is used to customize the user interface. | 
|  DefaultFilePath | Sets and returns the default path used when files are opened. | 
|  DelayCompute | Specifies whether or not to suspend the computing process. | 
|  DisplayAlerts | Enables or disables the display of alerts and messages. | 
|  DisplayFullScreen | Specifies whether or not the referenced Application object is maximized. | 
|  DisplayRecentFiles | Specifies whether or not the used file list is appended to the File menu of the referenced Application object. | 
|  DisplayRecentFilesCount | Sets and returns the number of files that are displayed in the most recently used (MRU) list. | 
|  Documents | Returns the collection of documents that are owned by the referenced Application object. | 
|  EdgeBarVisible | Specifies whether or not the Edge Bar is visible for the referenced Application object. | 
|  EnableStereo | Specifies whether or not the referenced Application object will support the creation of stereoscopic displays. | 
|  Environments | Returns a collection of Environment objects that are owned by the referenced Application object. | 
|  FeatureLibraryEvents | Returns the FeatureLibraryEvents object for the referenced Application object. | 
|  FileUIEvents | Returns the FileUIEvents object for the referenced Application object. | 
|  Height | Returns the height of the referenced object. | 
|  hWnd | Returns the window handle for the referenced object. | 
|  Insight | This read-only property returns the Insight object. | 
|  Interactive | Specifies whether or not the referenced Application object can be used interactively. | 
|  IsIdling |  | 
|  Left | Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container. | 
|  MailSession | Returns the MAPI mail session number. | 
|  Name | Returns the name of the referenced object. | 
|  NewFileUIEvents | Returns the NewFileUIEvents object for the referenced Application object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ProcessID | Returns the processID of the application. | 
|  ScreenUpdating | Determines if the screen updating is enabled or disabled. | 
|  SEECEvents |  | 
|  ShortcutMenuEvents | Returns the ShortcutMenuEvents object for the referenced Application object. | 
|  ShowStartupScreen |  | 
|  SolidEdgeInsightXT |  | 
|  SolidEdgeTCE |  | 
|  StatusBar | Sets and returns the caption text that is displayed in the referenced Application object. | 
|  StatusBarDelayUpdate | Specifies whether to immediately update the status bar or to defer the update to the idle loop. | 
|  StatusBarHeight | Returns the height of the status bar. | 
|  StatusBarPartCount | Sets and returns the number of parts or sections into which the status bar is divided. | 
|  StatusBarPartWidth | Returns the width of the current active part of the status bar. | 
|  StatusBarVisible | Specifies whether or not the status bar is visible. | 
|  Top | Sets and returns the distance from the top of the screen to the top of the referenced object or control. | 
|  UsableHeight | Returns the height of the usable vertical space in the application window. | 
|  UsableWidth | Returns the width of the usable horizontal space in the application window area. | 
|  UserName | Returns the name of the current user. | 
|  Value | Returns the name of the application, the value of a dimension, the value of a custom property, or the value of a variable. | 
|  Version | Returns the version number of the referenced Application object. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. | 
|  Width | Returns the width of the referenced object. | 
|  Windows | Returns a collection of Window objects. | 
|  WindowState | Returns or sets the state of the referenced window. |