| Solid Edge Framework Type Library > Application Object : SetGlobalParameter Method |
| Visual Basic |
|---|
Public Sub SetGlobalParameter( _ ByVal Parameter As ApplicationGlobalConstants, _ ByVal Value As Variant _ ) |
| Value | Description |
|---|---|
| seApplicationGlobalActivateAllParts | Activate All Parts |
| seApplicationGlobalAdminFileLocation | AdminFileLocation |
| seApplicationGlobalANSIInchToleranceFile | ANSI Inch Tolerance File |
| seApplicationGlobalANSIMetricToleranceFile | ANSI Metric Tolerance File |
| seApplicationGlobalApplicationDisplay | Application display mode for new windows |
| seApplicationGlobalApplyActivationOverridesToParts | Apply Activation Overrides To Parts |
| seApplicationGlobalApplySimplifyOverridesToParts | Apply Simplify Overrides To Parts |
| seApplicationGlobalApplySimplifyOverridesToSubAssemblies | Apply Simplify Overrides To SubAssemblies |
| seApplicationGlobalApplyStatusToLinks | Apply Status To Links |
| seApplicationGlobalAutomaticSave | Automatic Save |
| seApplicationGlobalAutomaticSaveTime | Automatic Save Time |
| seApplicationGlobalAutoSharpenLevel | Automatic sharpen level |
| seApplicationGlobalAvailableRootFolder | Available Root Folder |
| seApplicationGlobalBaselinedRootFolder | Baselined Root Folder |
| seApplicationGlobalChangedPartActivation | |
| seApplicationGlobalCheckInOnClose | Check In On Close |
| seApplicationGlobalColorActive | The color for active elements |
| seApplicationGlobalColorBackground | The color for the background |
| seApplicationGlobalColorConstruction | The color for construction elements |
| seApplicationGlobalColorDisabled | The color for disabled items |
| seApplicationGlobalColorFailed | The color for failed items |
| seApplicationGlobalColorHandle | The color for handles |
| seApplicationGlobalColorHighlight | The color for highlighted elements |
| seApplicationGlobalColorLiveSectionCenterline | |
| seApplicationGlobalColorLiveSectionEdge | |
| seApplicationGlobalColorLiveSectionOpacity | |
| seApplicationGlobalColorLiveSectionRegion | |
| seApplicationGlobalColorManagerCopyIndividualFaceColors | Color Manager Copy Individual Face Colors |
| seApplicationGlobalColorManagerShowAssemblyStyleOverrides | Color Manager Show Assembly Style Overrides |
| seApplicationGlobalColorManagerShowPartFaceColors | Color Manager Show Part Face Colors |
| seApplicationGlobalColorManagerUseIndividualPartStyles | ColorManager Use Individual Part Styles |
| seApplicationGlobalColorManagerUseToolsOptionsColorSettings | Color Manager Use Tools Options Color Settings |
| seApplicationGlobalColorProfile | The color for profiles, sketches and layouts |
| seApplicationGlobalColorRefPlane | Color RefPlane |
| seApplicationGlobalColorSelected | The color for items in the select set |
| seApplicationGlobalColorSheet | The color for the sheet |
| seApplicationGlobalColorSheetTab1 | Specifies the first of two alternating colors for the sheet tabs. |
| seApplicationGlobalColorSheetTab2 | Specifies the second of two alternating colors for the sheet tabs. |
| seApplicationGlobalCommandBarMode | Displays mode in command bar or quick bar. |
| seApplicationGlobalCurvatureCombDensity | Curvature Comb Density |
| seApplicationGlobalCurvatureCombMagnitude | Curvature Comb Magnitude |
| seApplicationGlobalCustomSettingFile | Custom Setting File |
| seApplicationGlobalDefaultSharpness | Default sharpness for new windows |
| seApplicationGlobalDisplayArcQuality | Display Arc Quality |
| seApplicationGlobalDisplayQuality | Display Quality |
| seApplicationGlobalDisplaySectionCaps | Enable the display of section caps with dynamic sections |
| seApplicationGlobalDisplayStatistics | Enable display timing statistics in the status bar |
| seApplicationGlobalDocumentNameFormula | |
| seApplicationGlobalDynamicTransition | Dynamic view transition smoothness |
| seApplicationGlobalECORootFolder | ECO Root Folder |
| seApplicationGlobalECRRootFolder | ECR Root Folder |
| seApplicationGlobalEnableDynamicTolerance | Enable dynamic tolerancing of facet data |
| seApplicationGlobalEnableThreadedDisplay | Enable multithreaded displays |
| seApplicationGlobalHideAllComponents | Hide All Components |
| seApplicationGlobalHoleSizeFile | Hole Size File |
| seApplicationGlobalInReviewRootFolder | In Review Root Folder |
| seApplicationGlobalInsightCacheLocation | Set InsightCacheLocation |
| seApplicationGlobalInsightFolderMappingFileLocation | Set InsightFolderMappingFileLocation |
| seApplicationGlobalInWorkRootFolder | Obsolete Root Folder |
| seApplicationGlobalISOToleranceFile | ISO Tolerance File |
| seApplicationGlobalLogFilesLocation | Set LogFilesLocation |
| seApplicationGlobalLookAheadVersion | LookAheadVersion |
| seApplicationGlobalMakeRevisionsObsolete | Make Revisions Obsolete |
| seApplicationGlobalObsoleteRootFolder | Obsolete Root Folder |
| seApplicationGlobalOfflineMode | Set OfflineMode |
| seApplicationGlobalOnLineHelpLocation | |
| seApplicationGlobalOpacityRefPlane | Opacity RefPlane |
| seApplicationGlobalOpenAsReadOnly3DFile | |
| seApplicationGlobalOpenAsReadOnly3DFile_IndirectFiles | |
| seApplicationGlobalOpenAsReadOnlyDftFile | |
| seApplicationGlobalOpenAsReadOnlyDftFile_IndirectFiles | |
| seApplicationGlobalOverlayColor | The color for visible edge overlay |
| seApplicationGlobalOverlayColorMode | The color mode for visible edge overlay [1=Absolute, 2=Relative] |
| seApplicationGlobalPackagedCollaborationRootFolder | Packaged Collaboration Root Folder |
| seApplicationGlobalPipeThreadfsFile | PipeThreadfsFile |
| seApplicationGlobalPrereleaseRootFolder | Prerelease Root Folder |
| seApplicationGlobalReleasedRootFolder | Released Root Folder |
| seApplicationGlobalRevisionDelimiter | Sets Revision Delimiter |
| seApplicationGlobalSaveMultiCADDatasettoTC | |
| seApplicationGlobalSearchScope | Set SearchScope |
| seApplicationGlobalSectionCurvatureCombDensity | |
| seApplicationGlobalSectionCurvatureCombMagnitude | |
| seApplicationGlobalSessionDraftOpenInactive | Draft inactive mode on open (boolean) |
| seApplicationGlobalSheetTabDisplayInfo | Specifies what information is displayed in the sheet tab : 0 = sheet number; 1 = sheet name; 2 = sheet number and sheet name |
| seApplicationGlobalSheetTabDisplayInfoSeparator | Specifies the separator string used between the sheet number and sheet name when both are displayed in the sheet tabs. |
| seApplicationGlobalShowUnitsInValueFields | Shows units of measure in value fields. |
| seApplicationGlobalSoftwareVHL | Enable software VHL/Disable hardware VHL |
| seApplicationGlobalStatusBarCmdFinder | Status Bar Command Finder |
| seApplicationGlobalStatusBarCommonViews | Status Bar Common Views |
| seApplicationGlobalStatusBarFit | Status Bar Fit |
| seApplicationGlobalStatusBarLookAtFace | Status Bar Look At Face |
| seApplicationGlobalStatusBarNamedViews | Status Bar Named View |
| seApplicationGlobalStatusBarPan | Status Bar Pan |
| seApplicationGlobalStatusBarPreviousView | Status Bar Previous View |
| seApplicationGlobalStatusBarRecordVideo | |
| seApplicationGlobalStatusBarRotateView | Status Bar Rotate View |
| seApplicationGlobalStatusBarSketchView | Status Bar Sketch View |
| seApplicationGlobalStatusBarSpinAbout | Status Bar Spin About |
| seApplicationGlobalStatusBarUploadToYouTube | |
| seApplicationGlobalStatusBarViewStyles | Status Bar View Styles |
| seApplicationGlobalStatusBarZoom | Status Bar Zoom |
| seApplicationGlobalStatusBarZoomArea | Status Bar Zoom Area |
| seApplicationGlobalStatusBarZoomSlider | Status Bar Zoom Slider |
| seApplicationGlobalStatusBarZoomTool | Status Bar Zoom Tool |
| seApplicationGlobalSystemInfo | Retrieve system information [readonly] |
| seApplicationGlobalTeamcenterFormula | |
| seApplicationGlobalTeamCenterMode | TeamCenter Mode |
| seApplicationGlobalTemplateRootFolder | Template Root Folder |
| seApplicationGlobalUpdateDraft | Update draft files also |
| seApplicationGlobalUploadOnClose | Upload On Close |
| seApplicationGlobalUseAllSimplifiedParts | Use All Simplified Parts |
| seApplicationGlobalUseAllSimplifiedSubAssemblies | Use All Simplified SubAssemblies |
| seApplicationGlobalUseDetailEnvelopeDisplayAsCircle | Show Detail Envelope as Circle when TRUE. |
| seApplicationGlobalUseDetailEnvelopeStandard | Use to set the Detail Envelope Standard Constants. Valid values are defined by enum DetailEnvelopeStandardConstants. |
| seApplicationGlobalUseDimensionStyleElementMapAngularCoordinateDim | |
| seApplicationGlobalUseDimensionStyleElementMapAngularDim | |
| seApplicationGlobalUseDimensionStyleElementMapBalloon | |
| seApplicationGlobalUseDimensionStyleElementMapBHC | |
| seApplicationGlobalUseDimensionStyleElementMapBlockLabels | |
| seApplicationGlobalUseDimensionStyleElementMapCallouts | |
| seApplicationGlobalUseDimensionStyleElementMapCenterline | |
| seApplicationGlobalUseDimensionStyleElementMapCenterMark | |
| seApplicationGlobalUseDimensionStyleElementMapChamferDim | |
| seApplicationGlobalUseDimensionStyleElementMapCircularDiameterDim | |
| seApplicationGlobalUseDimensionStyleElementMapConnectors | |
| seApplicationGlobalUseDimensionStyleElementMapCoordinateDim | |
| seApplicationGlobalUseDimensionStyleElementMapDatumFrames | |
| seApplicationGlobalUseDimensionStyleElementMapDatumPoints | |
| seApplicationGlobalUseDimensionStyleElementMapDatumTargets | |
| seApplicationGlobalUseDimensionStyleElementMapEdgeCondition | |
| seApplicationGlobalUseDimensionStyleElementMapFCF | |
| seApplicationGlobalUseDimensionStyleElementMapLeaders | |
| seApplicationGlobalUseDimensionStyleElementMapLinDim | |
| seApplicationGlobalUseDimensionStyleElementMapRadialDiameterDim | |
| seApplicationGlobalUseDimensionStyleElementMapRadialDim | |
| seApplicationGlobalUseDimensionStyleElementMapSTSymbols | |
| seApplicationGlobalUseDimensionStyleElementMapSymmetricDiameterDim | |
| seApplicationGlobalUseDimensionStyleElementMapWeldSymbols | |
| seApplicationGlobalUseDimensionStyleMapping | Use Dimension Style Mapping |
| seApplicationGlobalUseDrawingViewShowCroppingEdges | Show cropping edges when TRUE. |
| seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesHiddenByOtherParts | Show tangent edges that are hidden by other parts when TRUE. |
| seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesSelfHidden | Show the hidden tangent edges when TRUE. |
| seApplicationGlobalUseISOToleranceTable | Use ISO Tolerance Table when TRUE. Use ANSI Tolerance Table when FALSE. |
| seApplicationGlobalUseOnLineHelp | |
| seApplicationGlobalUserType | User Type |
| seApplicationGlobalZebraFolderMapping | Set ZebraFolderMapping |
| seApplicationGlobalZebraFormula |