Solid Edge Framework Type Library
BumpmapHeight Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: BumpmapHeight Property
Description
Sets and returns the apparent height of the bumps in the bump map used in the referenced FaceStyle object. If height is 0, the bumps have no apparent height. A typical value for height is 1.
Property type
Read-write property
Syntax
Visual Basic
Public Property BumpmapHeight As Single
See Also
FaceStyle Object
|
FaceStyle Members
Send comments
on this topic.