Solid Edge Framework Type Library
FaceStyle Object Members
Overview 
Public Methods
Public Method BeginPropertyBuffer
Public Method ClearSurfacePropertiesClears the surface properties for the referenced FaceStyle object.
Public Method ClearWireframePropertiesClears the wireframe properties for the referenced FaceStyle object.
Public Method DeleteDeletes the referenced object.
Public Method DetachDetach FaceStyle object from other objects.
Public Method FlushPropertyBufferFlushes the property buffer for the referenced FaceStyle or ViewStyle object.
Public Method GetAmbientReturns the red, green, and blue components of the ambient light for the referenced FaceStyle object.
Public Method GetBumpmapOffsetReturns the x and y offsets of the bump map used in the referenced FaceStyle object.
Public Method GetBumpmapScaleReturns the x and y scaling factors of the bump map used in the referenced FaceStyle object.
Public Method GetDiffuseReturns the red, green, and blue components of the diffuse color for the referenced FaceStyle object.
Public Method GetEmissionReturns the red, green, and blue components of the emission light for the referenced FaceStyle object.
Public Method GetSkyboxOrientationReturns the orientation of the skybox used in the referenced ViewStyle object.
Public Method GetSkyboxSideFilenameReturns the file name of the image used on one side of the skybox in the referenced FaceStyle object.
Public Method GetSpecularReturns the red, green, and blue components of the specular color for the referenced FaceStyle object.
Public Method GetTextureOffsetReturns the x and y offsets of the texture map used in the referenced FaceStyle object.
Public Method GetTextureScaleReturns the x and y scaling factors of the texture map used in the referenced FaceStyle object.
Public Method GetTextureTransparentColorReturns the RGB color that will be transparent in the texture map.
Public Method GetWireframeColorReturns the wireframe color for the referenced FaceStyle object.
Public Method HasSurfaceProperties
Public Method HasWireframeProperties
Public Method SetAmbientSets the red, green, and blue components of the ambient light for the referenced FaceStyle object.
Public Method SetBumpmapOffsetSets the x and y offsets of the bump map used in the referenced FaceStyle object.
Public Method SetBumpmapScaleSets the x and y scaling factors of the bump map used in the referenced FaceStyle object.
Public Method SetDiffuseSets the diffuse light for the referenced FaceStyle object.
Public Method SetEmissionSets the red, green, and blue components of the emission light for the referenced FaceStyle object.
Public Method SetSkyboxOrientationSets the orientation of the skybox used in the referenced ViewStyle object.
Public Method SetSkyboxSideFilenameSets the file name of the image used on one side of the skybox in the referenced FaceStyle object.
Public Method SetSkyboxSkyFileSets the name of the sky file used to define the skybox in the referenced FaceStyle object.
Public Method SetSpecularSets the red, green, and blue components of the specular color for the referenced FaceStyle object.
Public Method SetTextureOffsetSets the x and y offsets of the texture map used in the referenced FaceStyle object.
Public Method SetTextureScaleSets the x and y scaling factors of the texture map used in the referenced FaceStyle object.
Public Method SetTextureTransparentColorSets the RGB color that will be transparent in the texture map.
Public Method SetWireframeColorSets the wireframe color for the referenced FaceStyle object.
Public Method SkyboxClearClears the image from one side of the skybox in the referenced FaceStyle object.
Public Method SkyboxClearAllClears the images from all sides of the skybox in the referenced FaceStyle object.
Public Properties
Public Property AcceptsShadowsSets and returns a flag used in the referenced FaceStyle object. If the flag is true, other objects will cast shadows on the referenced object.
Public Property AmbientBlueSets and returns the blue component of the ambient color.
Public Property AmbientGreenSets and returns the green component of the ambient color.
Public Property AmbientRedSets and returns the red component of the ambient color.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BumpmapFileNameSets and returns the file name of the bump map used in the referenced FaceStyle object.
Public Property BumpmapHeightSets and returns the apparent height of the bumps in the bump map used in the referenced FaceStyle object. If height is 0, the bumps have no apparent height. A typical value for height is 1.
Public Property BumpmapInvertSets and returns a flag used on the bump map in the referenced FaceStyle object. If the flag is true, the bump map's bumps will invert, so that the high points will look like holes instead of bumps.
Public Property BumpmapMirrorXSets and returns a flag used on the bump map in the referenced FaceStyle object. If the flag is true, the bump map will be mirrored along the x axis.
Public Property BumpmapMirrorYSets and returns a flag used on the bump map in the referenced FaceStyle object. If the flag is true, the bump map will be mirrored along the y axis.
Public Property BumpmapOffsetXSets and returns the x offset of the bump map used in the referenced FaceStyle object.
Public Property BumpmapOffsetYSets and returns the y offset of the bump map used in the referenced FaceStyle object.
Public Property BumpmapRotationSets and returns the rotation of the bump map used in the referenced FaceStyle object, in degrees.
Public Property BumpmapScaleXSets and returns the x scaling factor of the bump map used in the referenced FaceStyle object.
Public Property BumpmapScaleYSets and returns the y scaling factor of the bump map used in the referenced FaceStyle object.
Public Property BumpmapUnitsSets and Returns the units used for bump map scaling. When it is set to 1, the scaling factors will be in world coordinates, which are the default. When it is set to 2, the scaling is in surface coordinates.
Public Property CastsShadowsSets and returns a flag used in the referenced FaceStyle object. If the flag is true, the referenced object will cast shadows on other objects.
Public Property DiffuseBlueSets and returns the blue component of the diffuse color for the referenced FaceStyle object.
Public Property DiffuseGreenSets and returns the green component of the diffuse color for the referenced FaceStyle object.
Public Property DiffuseRedSets and returns the red component of the diffuse color for the referenced FaceStyle object.
Public Property EmissionBlueSets and returns the blue component of the emission color for the referenced FaceStyle object.
Public Property EmissionGreenSets and returns the green component of the emission color for the referenced FaceStyle object.
Public Property EmissionRedSets and returns the red component of the emission color for the referenced FaceStyle object.
Public Property Flags
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property LineWidthSets and returns the line width (in paper space units) for the referenced object.
Public Property OpacitySets and returns the opacity for the referenced FaceStyle object. 1 is completely opaque, and 0 is completely transparent
Public Property ParentReturns the parent object for the referenced object.
Public Property ReflectivitySets and returns the reflectivity of the referenced FaceStyle object. Only used in advanced render modes like raytracing.
Public Property RefractionSets and returns the index of refraction for the referenced FaceStyle object. Only used in advanced render modes like raytracing.
Public Property ShininessSets and returns the shininess for the referenced FaceStyle object.
Public Property SkyboxAltitudeSets and returns the altitude of the skybox used in the referenced FaceStyle object.
Public Property SkyboxAzimuthSets and returns the azimuth of the skybox used in the referenced FaceStyle object.
Public Property SkyboxConeAngleSets and returns the cone angle of the skybox used in the referenced FaceStyle object.
Public Property SkyboxRollSets and returns the roll of the skybox used in the referenced FaceStyle object.
Public Property SkyboxTypeSets and returns the type of skybox used in the referenced FaceStyle object.
Public Property SpecularBlueSets and returns the blue component of the specular color for the referenced FaceStyle object.
Public Property SpecularGreenSets and returns the green component of the specular color for the referenced FaceStyle object.
Public Property SpecularRedSets and returns the red component of the specular color for the referenced FaceStyle object.
Public Property StipplePattern
Public Property StippleScale
Public Property StyleIDReturns the ID number of the referenced style object.
Public Property StyleNameSets and returns the name of the style that is applied to the referenced object.
Public Property TextureFileNameSets and returns the file name of the texture map used in the referenced FaceStyle object.
Public Property TextureMirrorXSets and returns a flag used on the texture map in the referenced FaceStyle object. If the flag is true, the texture will be mirrored along the x axis.
Public Property TextureMirrorYSets and returns a flag used on the texture map in the referenced FaceStyle object. If the flag is true, the texture will be mirrored along the y axis.
Public Property TextureOffsetXSets and returns the x offset of the texture map used in the referenced FaceStyle object.
Public Property TextureOffsetYSets and returns the y offset of the texture map used in the referenced FaceStyle object.
Public Property TextureRotationSets and returns the rotation of the texture map used in the referenced FaceStyle object, in degrees.
Public Property TextureScaleXSets and returns the x scaling factor of the texture map used in the referenced FaceStyle object.
Public Property TextureScaleYSets and returns the y scaling factor of the texture map used in the referenced FaceStyle object.
Public Property TextureTransparentSets and returns a flag used on the texture map in the referenced FaceStyle object. If the flag is true, the texture will be transparent wherever its pixels are the transparent color, otherwise the texture will be completely opaque.
Public Property TextureTransparentColorBlueSets and returns the blue component of the color that will be transparent in the texture map.
Public Property TextureTransparentColorGreenSets and returns the green component of the color that will be transparent in the texture map.
Public Property TextureTransparentColorRedSets and returns the red component of the color that will be transparent in the texture map.
Public Property TextureUnitsSets and returns the units used for texture scaling. When it is set to 1, the scaling factors will be in world coordinates, which are the default. When it is set to 2, the scaling is in surface coordinates.
Public Property TextureWeightSets and returns the weight of the texture map used in the referenced FaceStyle object. If weight is 1, the object's color comes entirely from the texture, and when weight is 0, the object's color comes entirely from the diffuse color.
Public Property TypeSpecifies the type of the object being referenced.
Public Property WidthSpace
Public Property WireframeColorBlueSets and returns the blue component of the wireframe color for the referenced FaceStyle object.
Public Property WireframeColorGreenSets and returns the green component of the wireframe color for the referenced FaceStyle object.
Public Property WireframeColorRedSets and returns the red component of the wireframe color for the referenced FaceStyle object.
See Also

FaceStyle Object

Send comments on this topic.