Solid Edge Framework Type Library
BumpmapMirrorY Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: BumpmapMirrorY Property
Description
Sets and returns a flag used on the bump map in the referenced FaceStyle object. If the flag is true, the bump map will be mirrored along the y axis.
Property type
Read-write property
Syntax
Visual Basic
Public Property BumpmapMirrorY As Long
See Also
FaceStyle Object
|
FaceStyle Members
Send comments
on this topic.