Solid Edge Framework Type Library
SkyboxAltitude Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: SkyboxAltitude Property
Description
Sets and returns the altitude of the skybox used in the referenced FaceStyle object.
Property type
Read-write property
Syntax
Visual Basic
Public Property SkyboxAltitude As Single
Remarks
Valid values are -90 to 90 degrees, inclusive.
See Also
FaceStyle Object
|
FaceStyle Members
Send comments
on this topic.