Solid Edge Framework Type Library
TextureMirrorX Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: TextureMirrorX Property
Description
Sets and returns a flag used on the texture map in the referenced FaceStyle object. If the flag is true, the texture will be mirrored along the x axis.
Property type
Read-write property
Syntax
Visual Basic
Public Property TextureMirrorX As Long
See Also
FaceStyle Object
|
FaceStyle Members
Send comments
on this topic.