Solid Edge Framework Type Library
TextureWeight Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: TextureWeight Property
Description
Sets and returns the weight of the texture map used in the referenced FaceStyle object. If weight is 1, the object's color comes entirely from the texture, and when weight is 0, the object's color comes entirely from the diffuse color.
Property type
Read-write property
Syntax
Visual Basic
Public Property TextureWeight As Single
See Also
FaceStyle Object
|
FaceStyle Members
Send comments
on this topic.