Application | Returns the active application object. |
Approve | Indicates the current recipient's approval. |
Approved | Indicates whether or not the current recipient has approved or rejected the associated document. |
AskForApproval | Indicates if an approval should be requested for each recipient. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Delivery | Sets and returns the delivery method used when routing. |
HasRouted | Specifies the current routing status of the referenced RoutingSlip object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Message | Sets and returns the message text for the referenced RoutingSlip object. |
Parent | Returns the parent object for the referenced object. |
Recipients | Sets the recipients on the referenced Routing Slip object. |
ReturnWhenDone | Determines whether or not the associated document is returned to the originator after completing its route. |
Status | Returns the status of the specified object. |
Subject | For RoutingSlip objects, sets and returns the subject of the routing slip mail message. For SummaryInfo objects, sets and returns a general description of the associated document. |
TrackStatus | Specifies whether or not tracking is to be activated for the referenced RoutingSlip object. |