ActiveSketch | Returns the active Sketch object. |
AddInsStorage | Returns an IUnknown pointer to the object that implements the IStorage corresponding to the add-in substorage for the referenced object. |
Application | Returns the active application object. |
AttributeQuery | Returns the AttributeQuery object. |
CreatedVersion | Returns the version of Solid Edge that was used to create the referenced document. |
Dirty | Specifies whether or not the referenced document has been modified since the last time it was saved. |
DocumentEvents | Returns the DocumentEvents object for the referenced document object. |
FullName | Returns the name and path of the referenced object. |
HighlightSets | Returns the HighlightSets collection object for the referenced document object. |
InPlaceActivated | Specifies whether or not the referenced document is in-place activated. |
IsTemplate | Specifies whether or not the referenced document is a template. |
LastSavedVersion | Returns the version of Solid Edge that was used the last time the referenced document was saved. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Path | Returns the directory path name of the referenced document. |
Properties | For document objects, returns the PropertiesCollection colletion object. For Variables, sets and returns the variable properties. |
ReadOnly | Specifies whether or not the referenced document has been opened as read-only. |
RootStorage | Returns the IUnknown pointer to the object implementing the root storage of the referenced document. |
RoutingSlip | Returns the RoutingSlip object for the referenced document. |
SelectSet | Returns the current selection set for the referenced document. |
Status | Returns the status of the specified object. |
SummaryInfo | Returns a SheetSummaryInfo object to provide access to descriptive properties for the referenced document. |
Type | Specifies the type of the object being referenced. |
UndoSteps | This read-write Long property sets and returns the number of undo steps for the referenced document object. |
UnitsOfMeasure | Returns the UnitsOfMeasure object for the referenced document. |
Variables | Returns the Variables collection object for the referenced document. |
Windows | Returns the Windows collection object. |